Post Go back to editing

Transformer and Transistor

Thread Summary

The user inquires about substituting the PSMN075-100MSEX MOSFET with the BUK9M60-100LX and using a transformer with common mode chokes (S558-5999-T7-F) instead of the recommended Wurth 7490100143. The final answer suggests verifying the MOSFET's SOA against the LTC9102/LTC9103 foldback curves and testing the circuit. Common mode chokes are problematic for the LTC9103 as they can distort low-frequency/DC signaling, leading to signal integrity issues or communication failure. Alternative MOSFETs tested and approved by ADI include the SI7322ADN-T1-GE3 and DMT10H015LFG-7, available at Digikey.
AI Generated Content
Category: Hardware
Product Number: LTC9103

The datasheet strongly suggests PSMN075-100MSEX for the transistor and a 10/100 Mbps transformer without common mode chokes for isolation.  Wurth 7490100143 is given as an example.

Both of these components are difficult to source.

BUK9M60-100LX from Nexperia seems to be very similar in parameters to PSMN075-100MSEX.  Would this be a valid alternative?

For the transformer, S558-5999-T7-F from Belfuse is the same footprint, but it has common mode chokes.  Why are common mode chokes and issue for this application?