I can change COUT and check the PM and GM on LTPowerCAD.
I could not find the place to change COUT and check PM/GM at the same time on PowerStudioDesigner.
How can I do that?


LTM8003
Recommended for New Designs
The LTM8003 is a 40VIN, 6A peak, 3.5A continuous stepdown Silent Switcher μModule® (power module) regulator. Included in the package are the switching...
Datasheet
LTM8003 on Analog.com
I can change COUT and check the PM and GM on LTPowerCAD.
I could not find the place to change COUT and check PM/GM at the same time on PowerStudioDesigner.
How can I do that?


Hello hk22,
When you open Capacitor – Ceramic (Couta1) or Bulk (Coutb1) on the left side of the Analyze → Loop and Load Transient screen, the Actual Capacitance field appears.
When you enter a value there, the graph is updated automatically.
You do not need to press the ENTER key when entering the value, but it may take a few seconds for the graph to update automatically.
Regards,