The LTC4292 can be commanded over the control interface to turn on a port manually, without proper detection/classification.
If VEE is below the undervoltage lockout threshold (typ. -25V), can I still command the port to turn on manually. I understand proper 802.3 detection/classification will not work, but can I turn on the the output FET manually if VEE is -20V?
Edit Notes
changed wording[edited by: ninaleechie at 5:17 PM (GMT -4) on 20 Apr 2026]