Post Go back to editing

LTC4292 operation in undervoltage lockout

Thread Summary

The user asked if the LTC4292 can be manually commanded to turn on a port when VEE is below the undervoltage lockout threshold (-25V). The final answer states that this is not possible if the LTC4292 is in UVLO. For lower VEE voltages, the LTC9101-1/LTC9103 is recommended due to its lower VEE UVLO threshold.
AI Generated Content
Category: Hardware
Product Number: LTC4292

The LTC4292 can be commanded over the control interface to turn on a port manually, without proper detection/classification.  

If VEE is below the undervoltage lockout threshold (typ. -25V), can I still command the port to turn on manually.  I understand proper 802.3 detection/classification will not work, but can I turn on the the output FET manually if VEE is -20V?

Edit Notes

changed wording
[edited by: ninaleechie at 5:17 PM (GMT -4) on 20 Apr 2026]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.