Hi All
In the schematic of DC1856B, R22 and R23 are 10ohm but if you open the dsn file you see they are 10Kohm 0603.
Can anybody valid the right value?
from the Application note it is pobalby 10ohm
ThanKs
Ido
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
LTM4649
Recommended for New Designs
The LTM4649 is a complete 10A high efficiency switching mode step-down DC/DC μModule® regulator in a 9mm × 15mm × 4.92 BGA package. Included in the...
Datasheet
LTM4649 on Analog.com
Hi All
In the schematic of DC1856B, R22 and R23 are 10ohm but if you open the dsn file you see they are 10Kohm 0603.
Can anybody valid the right value?
from the Application note it is pobalby 10ohm
ThanKs
Ido