Hi All
In the schematic of DC1856B, R22 and R23 are 10ohm but if you open the dsn file you see they are 10Kohm 0603.
Can anybody valid the right value?
from the Application note it is pobalby 10ohm
ThanKs
Ido
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
LTM4649
Recommended for New Designs
The LTM4649 is a complete 10A high efficiency switching mode step-down DC/DC μModule® regulator in a 9mm × 15mm × 4.92 BGA package. Included in the...
Datasheet
LTM4649 on Analog.com
Hi All
In the schematic of DC1856B, R22 and R23 are 10ohm but if you open the dsn file you see they are 10Kohm 0603.
Can anybody valid the right value?
from the Application note it is pobalby 10ohm
ThanKs
Ido
Hello,
Apologies for the confusion. Both should be 10 Ohms.