Post Go back to editing

Subharmonic Oscillation

Category: Hardware
Product Number: LTC3786

Hi,

I am using this controller for my boost converter, LTPowerCAD file attached. Below are my requirements:

Vin = 8.75V, Vout = 12V, Iout = 18.5A, Pout = 220W

However, I am observing a symptom of subharmonic oscillation as shown in the scope shot below. There's no oscillation at no load but observed it when I increased the load, started to observe the oscillation at about ~3A. I tried to use 2.2uH, 3.3uH and 4.7uH inductor to change the inductor slope (since I do not have control on the internal slope compensation ramp) but the symptom is still observed. When I changed the sense resistor to 3mohm (from 2mohm), to increase the gain, with 2.2uH inductor. The symptom disappeared. I believed this is something related to the internal slope compensation. However, with 3mohm sense resistor, I am limited to only 25A current limit. Can you suggest what can be done to achieve the load current of >18.5A? The inductor I used is the XGL1313 series from Coilcraft, which has high Isat

Scopeshot: L = 3.3uH, Rsense = 2mohm, no load

Scopeshot: L = 3.3uH, Rsense = 2mohm, Iout = 17A

12VF 200W 2nd stage.zip

  • Hi,

    Here are some practical paths forward:

    1. Sense Resistor Tradeoff
    • Increasing Rsense (from 2 mΩ → 3 mΩ) improves stability because it increases the effective current ramp relative to the compensation ramp.
    • The downside is reduced current limit. If you need >18.5 A continuous, you’ll want to avoid clipping too early.

    Option: Use multiple parallel sense resistors to fine‑tune the effective value. For example, 2.5 mΩ may give you stability without cutting the current limit too much.

    1. Inductor Selection
    • Larger inductance reduces the inductor current ripple, which lowers the sensed slope and makes slope compensation less effective.
    • Smaller inductance increases ripple, which helps stability but increases conduction losses and ripple current stress.
    1. Loop Compensation

    Even though the oscillation looks like subharmonic instability, verify your compensation network. A poorly tuned error amplifier can exacerbate the symptom.

    • Try lowering crossover frequency (reduce bandwidth).
    • Ensure adequate phase margin at high load.
    • Try to reduce Rth -> reduce BW and check it might improve subharmonic oscilation

    Please provide your observations results.

    Regards,

    Harshal

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.