I have wired the LT3480 with an older package. Is the device capable of running to provide the required negative voltage? Similar queries have been asked for LT3970. I am seeing a 0V output when turned ON
Is there any error in this schematic?
| SLA Status | Assignee | Support Status |
|---|---|---|
| ⚠ 3179 hours | MBRApps1 |
Assigned |
LT3480
Production
The LT3480 is an adjustable frequency (200kHz to 2.4MHz) monolithic buck switching regulator that accepts input voltages up to 36V (60V maximum). A high...
Datasheet
LT3480 on Analog.com
I have wired the LT3480 with an older package. Is the device capable of running to provide the required negative voltage? Similar queries have been asked for LT3970. I am seeing a 0V output when turned ON
Is there any error in this schematic?