Post Go back to editing

Driving SHDN pin on LTC4367 with 3.3V logic gate

Thread Summary

The user asked if the SHDN pin on the LTC4367 can be driven by a 3.3V CMOS gate, given the 10mA max current capability of the CMOS gate and the 1mA max current requirement of the SHDN pin. The final answer confirms that this setup should work, as the SHDN pin will only draw a few nA, well within the 10mA capability of the CMOS gate.

View FAQ
AI Generated Content
Category: Hardware
Product Number: LTC4367

Can SHDN pin on LTC4367 be driven from the output of 3.3V CMOS gate?

Voltage levels are within specification.

There is a concern about maximum current (3.3V CMOS gate can source/sink 10mA). 

Datasheet for LTC4367 specifies max. 1mA for SHDN pin. However, internal structure (datasheet, pg.8, block diagram) of LTC4367 shows only input to inverter, no diode or typical statement like "...absolute voltage level can be exceeded if current is below xx mA...".

Parents
  • Hello,

    so far my understanding with the given sink/source current is this: The 10mA are max which can be delivered WHEN the receiving end asks for such amount of current. Here we have the easy scenario that the SHDN pin from the LTC4367 will only asks for currents way lower than the stated AbsMax value of 1mA (datasheet claims +-15nA for a given condition):

    And hence your 3.3V logic ate will be easily deliver the current and not force more current into the SHDN Pin from the LTC4367.

    So you will see flawless operation within your scenario. Did I got your question right?

Reply
  • Hello,

    so far my understanding with the given sink/source current is this: The 10mA are max which can be delivered WHEN the receiving end asks for such amount of current. Here we have the easy scenario that the SHDN pin from the LTC4367 will only asks for currents way lower than the stated AbsMax value of 1mA (datasheet claims +-15nA for a given condition):

    And hence your 3.3V logic ate will be easily deliver the current and not force more current into the SHDN Pin from the LTC4367.

    So you will see flawless operation within your scenario. Did I got your question right?

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.