Hello folks (LT8312)
This is related to current spikes observed during startup.
L=312uH and Pout=150W Vout=380V Vin=120VAC 600Hz (600Hz for simulation speed)
The coupled inductor is a WE high current type. Isat=5A (I am using the WE models supplied by Wuerth) see circuit.

During start up the gate turns off and on intermittently. see waveform.
Any idea where this originates?
It appears there must be a condition present on one of the control pins , which instructs the controller to switch off the cycle. Perhaps a dv/dt value which gets exceeded etc..?
Anyway I have added an RC filter to the Vin pin 20Ohm and 100pF to reduce noise reaching the Vin pin.
Plus I have added a 5 or 10 Ohm NTC in the feed line. (to simulate the NTC in the real circuit)
(Mind you for loads above 150W the NTC will be replaced w a bypass resistor that gets shorted once 380V is nearly reached)
Any ideas
Thank you
n012 = secondary Laux feeding Vin and DCM
gateQ1 = MOSFET
Id2-IU2 = the inductor current
Vss+out = voltage out