Post Go back to editing

Technical Question about LTC4367

Category: Hardware
Product Number: LTC4367

Hello,

I want to use LTC4367 on my project to provide protection against under voltage. Basically, I want to disable my DC-DC converter by pulling its EN pin to ground, and I believe this can be achieved with a direct connection between fault pin of LTC4367 and EN pin of the DC-DC converter. The EN pin is internally pulled up to the VCC. 

My question concerns the gate pin of the LTC4367. Since I will not switch the main power supply to the DC-DC converter, I don't need to control the MOSFETs. Should I leave the gate control pin floating? On the other hand, can you please help me with the UV resistor selection and configuration of LTC4367. As I stated, I will use only the under voltage detection feature. 

Thank you

Edit Notes

float --> fault
[edited by: YsnKcl at 2:03 PM (GMT -4) on 9 Mar 2026]
Parents
  • Hi Yasin,

     

    If you do not want to use the EN pin in your DC-DC converter to create a undervoltage protection, you can disable it and use LTC4367 on your project for undervoltage lock out (UVLO). 
     

    However, I need a bit of clarity regarding your project:


    Which DC-DC converter are using?
    why do you want extra LTC4367 to achieve the UVLO, whereas, the EN pin from the DC-DC can actually be used to achieve a UVLO by connecting a resistor divider to it.

     

Reply
  • Hi Yasin,

     

    If you do not want to use the EN pin in your DC-DC converter to create a undervoltage protection, you can disable it and use LTC4367 on your project for undervoltage lock out (UVLO). 
     

    However, I need a bit of clarity regarding your project:


    Which DC-DC converter are using?
    why do you want extra LTC4367 to achieve the UVLO, whereas, the EN pin from the DC-DC can actually be used to achieve a UVLO by connecting a resistor divider to it.

     

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.