Hi,
I have the following circuit for the LT8302 simulated and correctly displaying +/-12V outputs but I just got prototype boards in for testing and once power was applied the LT8302 did not regulate the Secondary side of the transformer to +/-12V as expected but instead I see +/-24V on the output. After removing all devices except for the minimum load (LEDS) from the +/-12V rails the device still doesn't regulate the output correctly.
Is this configuration not valid with connection of P.6 and P.10 on the transformer T1 (connected as ground reference). Does D3 need to be moved between T1 P.10 and the ground reference for proper operation of the device?
Transformer utilizes is a 1.33:1:1 Wurth PN: 7491195212 which has 21uH coil inductance. Any feedback to help debug is greatly appreciated.
Thanks,
Sean