Post Go back to editing

Vbias voltage & SS pin

Category: Hardware
Product Number: LTM8048

Hi,

I am designing a power stage using the LTM8048 isolated uModule and have a question regarding the BIAS and SS pin connections as specified in the datasheet.

In the Absolute Maximum Ratings section, the SS pin is listed with a maximum allowable voltage of 5 VDC. However, in Table 1b (Recommended Components/Configurations), for VIN = 9 V to 15 V, the recommended connection is to tie BIAS = VIN. Under this configuration, the SS soft-start capacitor will be charged from the BIAS rail, which in this case is at VIN, potentially exceeding 5 V.

This appears to violate the stated absolute maximum rating for the SS pin. Could you clarify how the recommendation to connect BIAS = VIN is reconciled with the 5 V maximum on the SS pin?

Thank you for your assistance!!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.