Post Go back to editing

LED Display driver with high output current

Category: Hardware
Product Number: MAX6952EPL+, MAX6952

Is it possible to drive multiple LED's in series via the O0 to O23 outputs of the MAX6952EPL+ LED Display Driver?

I am trying to upgrade a large matrix display panel, which has 4 lines each with four 5 X 7 LED arrays. Each 'pixel' of the arrays comprises 5 LED's in series, to give high brightness.

The old system has an adequate power supply to drive all 560 LED's, just not sure how to implement an interface between the panels and the MAX6952's.  

Edit Notes

Video not relevant
[edited by: Denatec at 5:37 PM (GMT -5) on 3 Mar 2026]

Thread Notes