Hallo.
Sorry if this is placed wrong, but i could not find a better place.
If i use the LTC4287 it has a possibility to gate 2 pairs of FET's, but would it be possible to gate to pairs of Back-2-Back FET's to have reverse protection as well ?
I am gonna use the device to switch between 28V, 13A in put and 56V, 13A input, and for obvious reasons these 2 should NOT see each other.
If it is possible, what would be the best approach ?
Sincerely
Klavs Rommedahl.