Post Go back to editing

Vfb and Vioc when connected to a SEPIC

Category: Datasheet/Specs
Product Number: LT3041

Hello 

I have some questions related to building  LT3041 arrays in Voic configuration...(Assume R1=Vfb resistor, R3 = limit Vmax, and R2 )

1. Is it correct to assume that the value of Vref in any Vioc type scenario (in this case its LT3759 with +1.6V = Vref and -0.8V for negative) represents ultimately the Voic limit?

If Voic=Vfb(R1+R2/R1) then the smallest ratio is when R2 = 0. Which then sets Voic = Vfb.

Please advise 

2. When calculating the proper R3 values (for establishing an upper ceiling for Vmax-in)

What specific value is to be applied to Isink ? What is a good practice?  Could you please explain thank you.

R3 = Vmax - Vfb(R1+R2/R1) / (Vfb/R1+ Isink) 
Basically here it says that if R2 is zero then R3 is basically V(max)-V(fb) divided by the sum of I(sink) and I(R1).
For our initial prototype I had assumed 250uA as max I(sink) current. 
3. if we assume an inverting configuration then Vfb becomes -0.8V (with the sister chip LT3099)
Which ostensibly would reduce Vioc significantly in the negative array  (and reduce power loss etc.)
Is there a way to reduce Vioc in the positive regime?
Hope this makes sense.
Please elaborate. Thank you

Parents
  • Hi there 

    I have just finished a thread w. ADI LT SPICE support and it appears there is a serious bug in the way the LT3099 model gets executed on ARM M1/2 chips. 

    (Is it broader than the specific LT3099 model..? IDK. They requested more data etc. suffice to say - its a bug ) 

    The model essentially flows source currents in the wrong direction and much too high. Causing the model to misrepresent what's actually happening in the chip. My crossover instance of LT Spice works just fine. But I am Mac guy...I have a WIN11 machine for PSPICE and other WIN only dev stuff, but not a fan. Anyway just wanted to share in case someone else scratches their head over models not converging/working.

    Kind Regards 

Reply
  • Hi there 

    I have just finished a thread w. ADI LT SPICE support and it appears there is a serious bug in the way the LT3099 model gets executed on ARM M1/2 chips. 

    (Is it broader than the specific LT3099 model..? IDK. They requested more data etc. suffice to say - its a bug ) 

    The model essentially flows source currents in the wrong direction and much too high. Causing the model to misrepresent what's actually happening in the chip. My crossover instance of LT Spice works just fine. But I am Mac guy...I have a WIN11 machine for PSPICE and other WIN only dev stuff, but not a fan. Anyway just wanted to share in case someone else scratches their head over models not converging/working.

    Kind Regards 

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.