Hello,
we are using the LT3507A to generate with the Input voltage (10 - 32 Volt) the three output Voltages 5 Volt, 3,3 Volt and 1,35 Volt.
We have an voltage drop of the input voltage supply from 32 volts to 15 volts (see yellow signal in screenshot). Then all of the three output voltages drops, too. In the Screenshot the purple signal represents the 5 Volt. The 5 Volts decreased to 2.4 Volts.
The switch node (light blue signal in screenshot) stop to work for a little while. Then the LT3507A starts again to work and the voltages increase again.
The processor, which are powered by these three voltages, stop working proper.
Is there a way to figure out why the LT3507A behaves like this?