Hello,
I've used the LTspice LT8708 example circuit and stripped down most features to test basic functionality of the IC.
The problem I'm having is that Vout isn't being regulated and rises to match Vin no matter what the voltage on FBOUT pin is.
The only other change I made was replacing output voltage source asserting Vout with load resistor.
I have two questions:
1. Did I make any mistake in the circuit to explain this behavior
2. Was LT8708 model not set up to function without asserting output voltage with voltage source as shown in the example circuit?
Thanks you!