Hello,
I would like to know what the failure mode for MAX17613 is like when the input voltage exceeds 65V or when short circuit currents exceeds 3Amps.
Regards,
Gautam Modumudi.
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
MAX17613C
Production
The Olympus series of ICs is the industry's smallest and most robust integrated system protection solution. The MAX17613A/MAX17613B/MAX17613C adjustable...
Datasheet
MAX17613C on Analog.com
Hello,
I would like to know what the failure mode for MAX17613 is like when the input voltage exceeds 65V or when short circuit currents exceeds 3Amps.
Regards,
Gautam Modumudi.
Hi Gautam,
The recommended maximum operating voltage for MAX17613C is +60V. It can protect the overvoltage up to +60V and negative tolerance of up -65V. and maximum current of 3A. your system must adhere to this limits for MAX17613C not to fail.
Its work is to protect against too much current, too much voltage, too low voltage, and reverse polarity protection.
I hope that clarifies things.