Post Go back to editing

LTC3350 refuses to charge

Category: Hardware
Product Number: LTC3350
Software Version: Not Applicable

I have a circuit using LTC3350 that is showing odd behavior and wonder if anyone could help me resolve the issue?

When Vin is increased from 0V to 12V the capacitors do not start charging. This behavior is consistent across all boards. The prototype worked reliably, but maybe this was a fluke?

When probing the design to try to find the issue I have found that touching the PFI pin sometimes kicks the design into life and the capacitors then charge perfectly.

Looking at the SW node, as I gradually increase Vin from 0V to 12V the SW node starts switching when I reach ~5V (at 500KHz as expected). However when I get past 11V it suddenly stops and the charger sits there doing nothing (see images)

I've run out of things to try! I can't see anything wrong with the schematic, maybe I'm missing something?

The design intent is as follows:

1/ Vcap ~10V

2/ Switches over to back-up mode when Vin falls below ~9.9V

3/ Charge current limit set to 4A, but total current limited to 640mA (expectation is ~150mA load and 500mA left over for charging)

4/ Backup voltage is 12V

Parents
  • Hello,

    I am glad progress is being made on this. I have not seen the RSNSC affect the ability to charge like this before. This might have to do with the fact that RSNSC adjusts the peak current to provide an average charge current in charge mode. With the peak current much higher than the RSNSI limit, I expect the peak current limit is being reached before the RSNSI has a chance to react. That is my theory but will need to investigate. Most typical designs have an input current limit 1A or greater. 

    The other possibility is that the larger peak current creates more noise and is causing noise on the VCC2P5 pin. I have seen issues with noise on the VCC2P5 regulator causing odd behavior like this before.  One way to test this out is to remove C11, place it on top of the IC and connect it directly between the SGND and VCC2P5 pins.

Reply
  • Hello,

    I am glad progress is being made on this. I have not seen the RSNSC affect the ability to charge like this before. This might have to do with the fact that RSNSC adjusts the peak current to provide an average charge current in charge mode. With the peak current much higher than the RSNSI limit, I expect the peak current limit is being reached before the RSNSI has a chance to react. That is my theory but will need to investigate. Most typical designs have an input current limit 1A or greater. 

    The other possibility is that the larger peak current creates more noise and is causing noise on the VCC2P5 pin. I have seen issues with noise on the VCC2P5 regulator causing odd behavior like this before.  One way to test this out is to remove C11, place it on top of the IC and connect it directly between the SGND and VCC2P5 pins.

Children
No Data