Post Go back to editing

LTC3350 refuses to charge

Category: Hardware
Product Number: LTC3350
Software Version: Not Applicable

I have a circuit using LTC3350 that is showing odd behavior and wonder if anyone could help me resolve the issue?

When Vin is increased from 0V to 12V the capacitors do not start charging. This behavior is consistent across all boards. The prototype worked reliably, but maybe this was a fluke?

When probing the design to try to find the issue I have found that touching the PFI pin sometimes kicks the design into life and the capacitors then charge perfectly.

Looking at the SW node, as I gradually increase Vin from 0V to 12V the SW node starts switching when I reach ~5V (at 500KHz as expected). However when I get past 11V it suddenly stops and the charger sits there doing nothing (see images)

I've run out of things to try! I can't see anything wrong with the schematic, maybe I'm missing something?

The design intent is as follows:

1/ Vcap ~10V

2/ Switches over to back-up mode when Vin falls below ~9.9V

3/ Charge current limit set to 4A, but total current limited to 640mA (expectation is ~150mA load and 500mA left over for charging)

4/ Backup voltage is 12V

Parents
  • Thanks MartyM,

    Those are things that I can try and see if they make any difference. It is a 2-layer board and the bottom side is all GND. I can add capacitance on the bottom side of the board, directly between the pin 23 2V5 via and the GND vias. I'll take a 2V5 measurement with and without this capacitor. If that makes no difference I'll try your other suggestions.

    Thanks again

Reply
  • Thanks MartyM,

    Those are things that I can try and see if they make any difference. It is a 2-layer board and the bottom side is all GND. I can add capacitance on the bottom side of the board, directly between the pin 23 2V5 via and the GND vias. I'll take a 2V5 measurement with and without this capacitor. If that makes no difference I'll try your other suggestions.

    Thanks again

Children
No Data