Post Go back to editing

External load to BIAS voltage

Thread Summary

The user inquired about using the BIAS voltage (1.8V) from the MAX42402 to power a small buffer, which requires up to 0.5mA. The final answer indicates that the BIAS supply is not intended for external loads beyond the 20kΩ pull-up for the PGOOD output, as it is critical for the internal operation of the MAX42402.
AI Generated Content
Category: Datasheet/Specs
Product Number: MAX42402

Hi,

the buck regulator MAX42402 includes an internal LDO that powers the BIAS voltage (1.8V). Even though the datasheet shows that this voltage can be used to supply the pull-up connected to the open-drain PGOOD output, the maximum current that may be drawn from the BIAS supply is not specified.

Is it allowed to use the BIAS voltage for more peripheral circuitry? In my application I'd like to power a small TinyLogic buffer with it (several µA of static current needed, max. below 0.5mA).

Is this approach feasible or is not advised to load the BIAS supply externally with more than the shown 20k pull-up?

Best regards,
Thomas

  • Hello, the Bias is not intended to be used for other purpose aside from the PGOOD pull up as stated in the datasheet. Loading the BIAS pin externally beyond the shown 20kΩ pull-up is not explicitly advised. Since the BIAS regulator is critical for the internal operation of the MAX42402, excessive external loading could potentially disrupt device performance or reliability.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.