Post Go back to editing

Freewheeling Diode instead of bottom side mosfet

Thread Summary

The user inquired about replacing the bottom-side MOSFET with a Schottky diode in a buck converter using the LT3845A, aiming for space and cost reduction. The final answer confirmed that this is possible, with the diode's cathode connected to SW and the anode to ground, and the BG pin can be left floating. However, the BURST_EN pin must be grounded to disable burst mode, which is necessary for the diode replacement.
AI Generated Content
Category: Hardware
Product Number: LT3845A
Dear All,
I need an information about buck converter using LT3845A.
In case of DC/DC converter with Vin=15V and Vout=3.3V@500mA, is it possible to replace the bottom side mosfet with a diode (leaving floating pin BG?
This for space and cost reduction.
Thanks in advance for your gently reply
Stefano
Parents
  • Hi Anthonyuche, 

    thank you very much for your gently reply.

    Actually I connected the BURST_EN pin to Vcc, by analogy with the RH3845MK (which does not have the BURST function). This is in the case of future space applications.

    If I leave the BURST function disabled, is it not possible to replace the low MOSFET with a diode?

    Thanks in advance for your support.

    Kind Regards

    Stefano

Reply
  • Hi Anthonyuche, 

    thank you very much for your gently reply.

    Actually I connected the BURST_EN pin to Vcc, by analogy with the RH3845MK (which does not have the BURST function). This is in the case of future space applications.

    If I leave the BURST function disabled, is it not possible to replace the low MOSFET with a diode?

    Thanks in advance for your support.

    Kind Regards

    Stefano

Children
No Data