I want to use the MAX77504 Buck SMPS device in a battery operated design that is very current efficiency sensitive. The device will be asleep most of the time drawing 1-2ma. When it awakes up it will draw around 1A of current. Will the MAX77504 work well with a sleep mode current of 1-2ma? The simulator will only allow a min load current of 300ma. Is there a better device for this application?
William Sheppard
wdsheppard@earthlink.net