Post Go back to editing

Paralleling P-MOSFETs for larger current handling

Thread Summary

The user inquires about using the LTC2954CTS8-2 to control two MOSFETs in parallel for increased current handling. The final answer confirms that the LTC2954-2 can drive two MOSFETs in parallel, noting its open-drain EN̅ output can sink around 500uA, but a pull-up resistor is required to ensure proper turn-off of the FETs.
AI Generated Content
Category: Hardware
Product Number: LTC2954

I am planning to use the ltc2954cts8-2, the p-mosfet version to control a circuit.

i was thinking of paralleling 2 mosfets to drive the circuit with an increased current handling capability.

does the chip have enough gate driveability to work with 2 mosfets as we are practically just bringing the voltage to 0?

Parents
  • Hi  ,

    Yes, in principle, the LTC2954-2 can drive two mosfets gates in parallel but note that LTC2954CTS8‑2 EN̅ output is an open‑drain control and only meant as an enable signal, not a strong MOSFET gate driver. Since its open-drain, a pull up is typically required at the output. Too large of a pull up can slow down the turn-off of your FETs.
    The LTC2954-2 only needs to pull the gate node low (asserted) and then release it (deasserted), note that the EN output is specified sinking around 500uA.
    Best regards,
    Gaell
Reply
  • Hi  ,

    Yes, in principle, the LTC2954-2 can drive two mosfets gates in parallel but note that LTC2954CTS8‑2 EN̅ output is an open‑drain control and only meant as an enable signal, not a strong MOSFET gate driver. Since its open-drain, a pull up is typically required at the output. Too large of a pull up can slow down the turn-off of your FETs.
    The LTC2954-2 only needs to pull the gate node low (asserted) and then release it (deasserted), note that the EN output is specified sinking around 500uA.
    Best regards,
    Gaell
Children
No Data