Post Go back to editing

Detection signature

Thread Summary

The user's circuit is not starting due to an invalid detection signature, which should mimic a 25kOhm resistor with less than 120nF parallel capacitance. The LT4320 is intended for auxiliary input bridges; the LT4321 should be used for PoE input bridges. Removing or bypassing the LT4320 and ensuring C113 is 47nF may resolve the issue. The circuit also requires a bridge on both pairsets.
AI Generated Content
Category: Hardware
Product Number: LT4295

I measured Pout as shown in captured waveform. The peak reach only about 7V. The circuit not able to start. The converter will operation if i apply 48V after the pass FET (Vin)

Any idea why it is not starting? Thanks

Parents
  • Hello,

    Your circuit is presenting an invalid detection signature, meaning it doesn't look like a 25kOhm resistor with less than 120nF of parallel capacitance. First, the LT4320 is intended for auxiliary input bridges, as shown on page 25 of the LT4295 datasheet. You should use the LT4321 for PoE input bridges as it is designed to not corrupt the detection signature. You can try removing or bypassing the LT4320 as the MOSFETs should act like silicon diodes with it removed to confirm the detection signature becomes valid. Second, C113 should be reduced to 47nF but this likely isn't causing this issue. You also need a bridge on both pairsets which is why the LT4321 controls two full bridges. Right now V3 and V4 is floating.

    Best Regards,

    Eric

Reply
  • Hello,

    Your circuit is presenting an invalid detection signature, meaning it doesn't look like a 25kOhm resistor with less than 120nF of parallel capacitance. First, the LT4320 is intended for auxiliary input bridges, as shown on page 25 of the LT4295 datasheet. You should use the LT4321 for PoE input bridges as it is designed to not corrupt the detection signature. You can try removing or bypassing the LT4320 as the MOSFETs should act like silicon diodes with it removed to confirm the detection signature becomes valid. Second, C113 should be reduced to 47nF but this likely isn't causing this issue. You also need a bridge on both pairsets which is why the LT4321 controls two full bridges. Right now V3 and V4 is floating.

    Best Regards,

    Eric

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.