I measured Pout as shown in captured waveform. The peak reach only about 7V. The circuit not able to start. The converter will operation if i apply 48V after the pass FET (Vin)
Any idea why it is not starting? Thanks


KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
LT4295
Recommended for New Designs
The LT4295 is an IEEE 802.3af/at/bt-compliant powered device (PD) interface controller with a switching regulator controller. The T2P output indicates...
Datasheet
LT4295 on Analog.com
I measured Pout as shown in captured waveform. The peak reach only about 7V. The circuit not able to start. The converter will operation if i apply 48V after the pass FET (Vin)
Any idea why it is not starting? Thanks


Hello,
Your circuit is presenting an invalid detection signature, meaning it doesn't look like a 25kOhm resistor with less than 120nF of parallel capacitance. First, the LT4320 is intended for auxiliary input bridges, as shown on page 25 of the LT4295 datasheet. You should use the LT4321 for PoE input bridges as it is designed to not corrupt the detection signature. You can try removing or bypassing the LT4320 as the MOSFETs should act like silicon diodes with it removed to confirm the detection signature becomes valid. Second, C113 should be reduced to 47nF but this likely isn't causing this issue. You also need a bridge on both pairsets which is why the LT4321 controls two full bridges. Right now V3 and V4 is floating.
Best Regards,
Eric
thank you very much for clarification. I remove the LT4320 and short the gates to source on the bridge FET, it is working now.