if the VSYNC pin is not used to set device timing, how to set those reg to switch on the led?
KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
| SLA Status | Assignee | Support Status |
|---|---|---|
| ⚠ 5685 hours | Open | |
MAX25588
Recommended for New Designs
The MAX25588 is a 38-channel low-side driver. The integrated current outputs can sink up to 40mA LED current each. Device power comes from an external...
Datasheet
MAX25588 on Analog.com
if the VSYNC pin is not used to set device timing, how to set those reg to switch on the led?