Post Go back to editing

LT8316 Bias and FB loops

Category: Hardware
Product Number: LT8316

Hello Folks,

Finally made my design work. (LT8316 100-140VAC to +/-24V 50/100W)

Board controls line and load well. <50mV ripple

This isolated 24V flyback is the backbone for a series of 15/12/5/3.3v blades using the LT3759.

I have a few questions:

1. What do you recommend I do to contain the high bias levels.

I am using a Wuerth Flyback for +-24VDC 100W in my 100W design w. 122uH (750811749). Laux is 18-20V.

The bias climbs at PSS (periodic steady state) to 30-31VDC, which is below the 40V limit for Bias .

The LT8316 internal LDO generates 10V and so I am worried the chip has to dissipate unnecessary more power.

The LTSPICE simulation shows 20+volts but I am experiencing 30+V. see scope image.

My hunch is the system has inductive ringing somewhere caused by board design perhaps...

(As a possible solution I am experimenting w a 20/22V UniTVS to clamp the Vaux ringing which seems to be working. UniTVS to leave the negative pulse unaffected)

Any thoughts ?

Below the Bias with no TVS. (C3 is Vaux , C4 is bias - scope is 200MHz latest gen 14 bit)

As you can see the Vaux has a plateau of 20.565V but additional ringing causes the Bias to swell to 30V. 

Here after inserting uniTVS, reducing Bias to 22.8V (C1 is VdrainQ1 C4 is Bias)

2. Second question is related to Vfb

Based on the above LT8316 design I have started an alternative version using SSR (versus my original design uses PSR )

ADUM4195-1 feeding secondary to the FB pin (via a fine tune potentiometer), adding a secondary 5V regulator plus an HV network/transistors/zeners to reduce the primary power to 5V etc.. 

Obviously much more complex plus adding a several dollars to the BOM. That said the PSR is ok if the downstream stability requirements are not too stringent.

I have experimented w a one turn potentiometer in the PSR loop to see if the tolerance spread can be compensated after production etc..

but it appears this is causing enormous stability issues especially for the FB/VC loop. (frequency is not stable etc.)

Any thoughts about this??

3. See ripple 

How do I refine the output ripple with this LT8316 design?

The ripple RMS is around 40-60mV (about 0.2%). Ripple Vpp is 200-230mV. 

How can i address this and avoid having it flow downstream?

Thank you for your help.

  • Thank you for sharing details.

    Can you also provide pdf of your schematic clearly showing all connections of LT8316 and corresponding external components. 

  • Hello and thank you for looking at this.

    1. PDF attached shows the As-built Rev03.31

    PDF

    The design's aim is to produce +/-24VDC 100W PSS using the LT8316 chip and WE750811759 TXFR. 

    Vin: 100-240VAC

    Ripple<0.1%. Load Reg. <1% (10W to 90W)

    Efficiency target >90%

    2. Attached is also a corresponding LTSPICE circuit. 

    PSS4_LT8316_2x24V_100W_Rev003.31

    Some notes:

    1. Rsense set to 30m to get Pout=100W. At 20/25m the circuit will produce Pout=120W power.

    2. Ireg is softstart C24 = 100nF

    3. MOSFETs used are INFINEON: IPB65R115CFD7A or IPB60R180C7 (both are rated Vds=600V). LMK if you need the lib. files.

    4. Input EMI circuit not simulated 

    thank you

    PSS4_LT83XX_2x24V 120W_Rev003.31.asc

  • See below LT waveforms at Rload=10 (120W Pout) 

    The frequency at full power is about 129KHz. System in PSS in BCM mode. (140kHz cutoff plus Rsense sets upper power limit)

    It appears the controller pushes the frequency up as it maintains BCM, while limiting max current flow. (to reduce Vfb error for a given Rload)

    My sense is the system can deliver substantially more power with a more capable transformer/MOSFET/RECT using this same architecture. (perhaps switch to SSR).

    I am planning to develop this into 100W/150W/200W 24V platform. (avoiding the cost/complexities of Forward or LLC converters - at least for now.)

    The fundamental strategy is to focus on +24VDC (100-200W), and avoid a negative -24V bus supply altogether,

    But using a buck/boost LT3759 blade (interchangeable) to generate a series of positive and negative supplies). 

    Please advise on my questions thank you.

    Kind regards 

  • Thank you for sharing the schematic and LTSPICE files. I will review them and get back to you. 

  • Finally made my design work. (LT8316 100-140VAC to +/-24V 50/100W)

     

    Board controls line and load well. <50mV ripple

    This isolated 24V flyback is the backbone for a series of 15/12/5/3.3v blades using the LT3759.

     

    I have a few questions:

    100W output power is right at max with flyback topology, I would look into using Forward topology 

    1. What do you recommend I do to contain the high bias levels.

    I am using a Wuerth Flyback for +-24VDC 100W in my 100W design w. 122uH (750811749). Laux is 18-20V.

    The bias climbs at PSS (periodic steady state) to 30-31VDC, which is below the 40V limit for Bias .

    The LT8316 internal LDO generates 10V and so I am worried the chip has to dissipate unnecessary more power.

    The LTSPICE simulation shows 20+volts but I am experiencing 30+V. see scope image.

    My hunch is the system has inductive ringing somewhere caused by board design perhaps...

    (As a possible solution I am experimenting w a 20/22V UniTVS to clamp the Vaux ringing which seems to be working. UniTVS to leave the negative pulse unaffected)

    Any thoughts ?

    I agree with ringing on Bias is most likely due to parasitic on Tertiary winding. This could include transformer and layout. Clamping the ringing would be a good start. 

    Below the Bias with no TVS. (C3 is Vaux , C4 is bias - scope is 200MHz latest gen 14 bit)

    As you can see the Vaux has a plateau of 20.565V but additional ringing causes the Bias to swell to 30V. 

    Here after inserting uniTVS, reducing Bias to 22.8V (C1 is VdrainQ1 C4 is Bias)

    Channel 4 showing Bias pin is not clearly visible in this plot, but based on your note it seems ringing has been reduced which is what I would expect. 

    2. Second question is related to Vfb

    Based on the above LT8316 design I have started an alternative version using SSR (versus my original design uses PSR )

    ADUM4195-1 feeding secondary to the FB pin (via a fine tune potentiometer), adding a secondary 5V regulator plus an HV network/transistors/zeners to reduce the primary power to 5V etc.. 

    Obviously much more complex plus adding a several dollars to the BOM. That said the PSR is ok if the downstream stability requirements are not too stringent.

    I have experimented w a one turn potentiometer in the PSR loop to see if the tolerance spread can be compensated after production etc..but it appears this is causing enormous stability issues especially for the FB/VC loop. (frequency is not stable etc.)

    Any thoughts about this??

    I believe you are looking into using Synchronous secondary rectifier mainly to improving efficiency. 

    You can take a look at LT8309 which is a secondary side synchronous rectifier driver

     See ripple 

    How do I refine the output ripple with this LT8316 design?

    The ripple RMS is around 40-60mV (about 0.2%). Ripple Vpp is 200-230mV. 

    How can i address this and avoid having it flow downstream?

    Thank you for your help.

    Between flyback and forward, forward converter has much lower output ripple.

    In flyback, output ripple depends on:

    1. Layout

    2. Output capacitance and ESR

    Output ripple can be reduced by adding output capacitors and looking at output capacitor ESR.

    You can also look into adding 2nd stage LC filter at the output

     

  • My response:: to your response.

    100W output power is right at max with flyback topology, I would look into using Forward topology 

    1. What do you recommend I do to contain the high bias levels.

    I am using a Wuerth Flyback for +-24VDC 100W in my 100W design w. 122uH (750811749). Laux is 18-20V.

    The bias climbs at PSS (periodic steady state) to 30-31VDC, which is below the 40V limit for Bias .

    The LT8316 internal LDO generates 10V and so I am worried the chip has to dissipate unnecessary more power.

    The LTSPICE simulation shows 20+volts but I am experiencing 30+V. see scope image.

    My hunch is the system has inductive ringing somewhere caused by board design perhaps...

    (As a possible solution I am experimenting w a 20/22V UniTVS to clamp the Vaux ringing which seems to be working. UniTVS to leave the negative pulse unaffected)

    Any thoughts ?

    I agree with ringing on Bias is most likely due to parasitic on Tertiary winding. This could include transformer and layout. Clamping the ringing would be a good start. 

    Below the Bias with no TVS. (C3 is Vaux , C4 is bias - scope is 200MHz latest gen 14 bit)

    As you can see the Vaux has a plateau of 20.565V but additional ringing causes the Bias to swell to 30V. 

    Here after inserting uniTVS, reducing Bias to 22.8V (C1 is VdrainQ1 C4 is Bias)

    Channel 4 showing Bias pin is not clearly visible in this plot, but based on your note it seems ringing has been reduced which is what I would expect. 

    I have started to characterize the Csnubber size. My measurements show the LC ringing (Leakage inductance)  is right at 4MHz. My original design used a 75p and R510. (-3dB at 4MHz). Basically in the time domain this capacitance must be higher to counter the resonance. At a frequency level this low pass corner (-3dB) needs to shift down toward 1MHz w an attenuation of 12-15dB at 4MHz etc. 

    Furthermore (this is relevant for the 50W design only) the Snubber Zener is currently set to 188V. Given the Vin,  N1/N2 ratio of 4, plus the output diodes plus the Vout i get about 280-300V. (Vin min vs Vin max). However the Zener TVS conducts only at about (Vin+ 188VZener which is over 330V). I am planning to further reduce the TVS working voltage from 188 to 150V and possibly to 130V to reset the leakage more efficiently. LMK what you think. 

    2. Second question is related to Vfb

    Based on the above LT8316 design I have started an alternative version using SSR (versus my original design uses PSR )

    ADUM4195-1 feeding secondary to the FB pin (via a fine tune potentiometer), adding a secondary 5V regulator plus an HV network/transistors/zeners to reduce the primary power to 5V etc.. 

    Obviously much more complex plus adding a several dollars to the BOM. That said the PSR is ok if the downstream stability requirements are not too stringent.

    I have experimented w a one turn potentiometer in the PSR loop to see if the tolerance spread can be compensated after production etc..but it appears this is causing enormous stability issues especially for the FB/VC loop. (frequency is not stable etc.)

    Any thoughts about this??

    I believe you are looking into using Synchronous secondary rectifier mainly to improving efficiency. 

    You can take a look at LT8309 which is a secondary side synchronous rectifier driver

    Yes LT8309 is a good choice. The ADuM4195 is targeted toward SSR feedback to the FB pin and not using the tertiary winding for voltage feedback. 

    Also eliminating the need for TC pin programing etc. since the diodes are not part of the loop.

    I have built a test harness for this and it works well. It assures +24VDC under all conditions,. and allows inserting a potentiometer into the loop. for tuning. etc. 

    This is only relevant for 100-140W when using the higher power Wuerth Flybacks. (It is the absolute limit of Flybacks I agree)

     See ripple 

    How do I refine the output ripple with this LT8316 design?

    The ripple RMS is around 40-60mV (about 0.2%). Ripple Vpp is 200-230mV. 

    How can i address this and avoid having it flow downstream?

    Thank you for your help.

    Between flyback and forward, forward converter has much lower output ripple.

    In flyback, output ripple depends on:

    1. Layout

    2. Output capacitance and ESR

    Output ripple can be reduced by adding output capacitors and looking at output capacitor ESR.

    You can also look into adding 2nd stage LC filter at the output

    Yes I have started to implement an LC filter in the output. (1uH and super low PANASONIC low ESR caps 1000uF w a 2Ohm || resistor to reduce startup current through the inductor.)

    Also at 200-220W we will be looking at synchronous Forward controllers. It is part of the PSS5 strategy.

    Much more complex design (high BOM costs) even if more efficient and less noisy. (at least 4 magnetics plus a half bridge switcher plus opto/icoupler etc.)

    thank you

  • Sorry for the "low pass" comment when referring to the snubber RC in series. (It is a high pass after all as it clamps the frequencies above its corner frequency)

    I am working on optimizing the PSS4 LT8316 50W and the 125W snubber system. More to follow thank you.