Hello,
I am trying to simulate the Figure 84 – Positive and Negative Variable Supply from the LT8582 datasheet, using:
-
LT8582 as dual boost / inverting converter
-
LT3041 as positive LDO
-
LT3099 as negative LDO
The goal is a bipolar supply, with a load mainly connected between VPOS and VNEG.
Target outputs:
-
VPOS ≈ +8 V
-
VNEG ≈ −6 V
I built the circuit in LTspice following Figure 84, including:
-
Coupled inductors (K = 0.99)
-
Schottky diodes (BAT54 / 1N5818)
-
EN and SHDN pins tied high
-
PGFB tied to IN (no fast-start required)
-
Schottky clamps to prevent VPOS going below GND
However, the circuit does not start or regulate in simulation:
-
out_positive ≈ 0 V -
out_negative ≈ 0 V -
SET pin currents in LT3041/LT3099 are essentially zero
-
LDO input rails remain near 0 V
A .op analysis shows VIN = 12 V is present, but the switching converter does not appear to generate the intermediate rails for the LDOs. A transient simulation (.tran startup) also shows no regulation.
I would like to ask:
-
Is Figure 84 expected to work directly in LTspice with the provided LT8582 / LT3041 / LT3099 models?
-
Are there specific enable / sequencing requirements in simulation that are not obvious from the datasheet?
-
Is a Schottky clamp or startup sequencing required for LT3041/LT3099 in LTspice?
-
Are there known limitations or required initial conditions for LT8582 bipolar configurations in LTspice?
I have attached my LTspice schematic and screenshots of the simulation results.
Thank you very much for your help.