LX1, CSN1 and CSP1 are rated at 0V -0.3V to Vin +0.3V, but there is no such pin as VIN. There is an "IN" pin which I supply with 5V so that the IC can start up, it then rises to 7 or 14V when the output comes up. The input at CSN1, CSP1 and MOSFET D is up to runs from 400mV to 35V.
MAX25431 has the same ambiguity in the datasheet, but LTC3789 does not.
An Engineers Perspective: Vintage and Veteran Car dynamo power management
Edit Notes
List two other ADI parts one also has the same ambiguity, the other datasheet is clear.[edited by: andrew-lohmann@home at 5:45 PM (GMT -5) on 20 Dec 2025]