Post Go back to editing

LTC4041 - Unexpected low charge current

Category: Hardware

Hello,

I’m experiencing an issue with the LTC4041.

I want to charge two supercapacitors (2 × 50 F / 2.7 V in series) at 2 A. I’ve attached the circuit diagram.

Currently, there is no load connected to Vsys. However, the charging process takes a very long time, and the charge current only increases very slowly. The desired 2 A is reached only shortly before the final charge voltage. This can be clearly seen in the attached oscilloscope screenshot.

The first trace (blue) shows Vsys. The circuit is powered by a lab power supply set to 5.1 V, with a current limit of 5 A, so that should not be an issue.

The second trace (red) shows the current; 1 V corresponds to approximately 1 A. You can see that the current rises gradually throughout the entire charging period. I expected it to be limited initially and then switch to the full 2 A.

The green trace shows the voltage at Scap.

The third trace (yellow) shows the voltage at the PROG pin.

The entire charging process takes more than one minute, which is too long for my application—this is exactly why I chose the LTC4041, to charge as quickly as possible with a constant 2 A.

Any help would be greatly appreciated!

Edit Notes

Added color "red" to the desciption of the second trace.
[edited by: AndreWippich at 6:50 AM (GMT -5) on 17 Dec 2025]
  • Hi,

     

    Just looking at the capacitor voltage, the part seems to be working as expected. If you have a constant 2A charging current, two 50F caps, and assuming ideal conditions, I expect the caps to fully charge in around 56s. The math is included below:

     

    For a capacitor, I = C * dV/dt 

    dV/dt = I / C 

    dV/dt = 2A / 25F (two 50F caps in series equivalent to one 25F cap)

    dV/dt = 1/12.5 V/s

     

    Time to charge assuming constant current:

    (Vfull - Vempty) / (dV/dt) ~= tCharge

    (4.5 - 0) / (1/12.5 V/s) = 4.5 * 12.5 = 56.25s = tCharge

     

    The slope of the cap voltage waveform you sent appears to match up exactly with our expectation assuming a constant current (2V / 25s, or 1/12.5 V/s). 

     

     

     

     

    Your caps also seem to charge in roughly 60s, which again aligns with the math above. In practice, the charging time takes a little longer due to parasitics, cap balancing, and other non-idealities. 

     

    If you need faster charging time, you may want to explore a part like the LTC3350, which allows for higher charging currents due to the external power FETs

     

    LTC3350 Datasheet and Product Info | Analog Devices

     

    Best,

    Blaise

  • Hi,

     

    Just looking at the capacitor voltage, the part seems to be working as expected. If you have a constant 2A charging current, two 50F caps, and assuming ideal conditions, I expect the caps to fully charge in around 56s. The math is included below:

     

    For a capacitor, I = C * dV/dt 

    dV/dt = I / C 

    dV/dt = 2A / 25F (two 50F caps in series equivalent to one 25F cap)

    dV/dt = 1/12.5 V/s

     

    Time to charge assuming constant current:

    (Vfull - Vempty) / (dV/dt) ~= tCharge

    (4.5 - 0) / (1/12.5 V/s) = 4.5 * 12.5 = 56.25s = tCharge

     

    The slope of the cap voltage waveform you sent appears to match up exactly with our expectation assuming a constant current (2V / 25s, or 1/12.5 V/s). 

     

     

     

     

    Your caps also seem to charge in roughly 60s, which again aligns with the math above. In practice, the charging time takes a little longer due to parasitics, cap balancing, and other non-idealities. 

     

    If you need faster charging time, you may want to explore a part like the LTC3350, which allows for higher charging currents due to the external power FETs

     

    LTC3350 Datasheet and Product Info | Analog Devices

     

    Best,

    Blaise

  • on Dec 19, 2025 3:00 AM Contains AI Generated Content
    0
    Hello Blaise,
    thank you very much for your response! You are absolutely right — the charging behavior is completely correct. I really appreciate that you explained it in such detail!
    I had a silly misconception because I expected a constant input current of 2 A on the supply side of the circuit.
    I asked Copilot to formulate an explanation for other users:
    The input current is not constant because the LT4041 regulates a constant output current, not input current. As the capacitor voltage rises, the output power increases linearly (P = V × I). Since the input voltage is fixed, the input current must rise proportionally to supply the growing output power. This is why the input current starts low (Pout = 0,5V * 2A) and gradually increases until it reaches its maximum near the end of the charge cycle (Pout = 4,5V * 2A).
    Bye,
    Andre

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.