KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
LT3845A
Recommended for New Designs
The LT3845A is a high voltage, synchronous, current mode controller used for medium to high power, high efficiency supplies. It offers a wide 4V to 60V...
LT3845A on Analog.com
We need to verify that the component is AEC-Q100 compliant.
For what it is stated in your web, it seems it is:

But we could not find the exact information in the page nor in the datasheet of the product.
Thanks a lot!
LT3845A is not available in an automotive grade. I think that what is being stated on our website is that all devices that we develop specifically for automotive applications will have full AEC-Q100 qualification.
If you want further assistance, we can help you to identify a device with AEC-Q100 qualification. If you can provide us some target specs such as input voltage, output voltage, target switching frequency and any special features that you require, we can look for an alternative.
I have not heard back from you and will assume that you do not need further assistance.