Post Go back to editing

Clarification on VPRG1, VPRG2 pin configuration for resistor divider feedback control.

Category: Hardware
Product Number: LTC7138

Hello there, 

 I'm planning to use LTC7138 with resistor divider feedback control. 

While I checked the datasheet, Fig 6 mentioned VPRG1, VPRG2 to connect to GND. 

 

But in the application section figure 11, VPRG1 connects to SS (Which is supposed to be a 5V fixed configuration). 

Kindly suggest which configuration to follow for the external voltage divider based VFB method. Thanks heaps! 

  • Hi,

     

    It depends on what output voltage the chip will be used to generate. For high output voltages (>10V), it is recommended to use the schematic in Figure 11, where the Vfb is set to the fixed 5V configuration, and then external resistors are added to adjust the output voltage to a voltage above 5V. Otherwise, the schematic in Figure 6 can be used.

     

    Thanks!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.