Post Go back to editing

Maximum FAULT Pin Sink Current (LTC4365)

Thread Summary

The user inquires about the sink current capability of the nFAULT pin on the LTC4365, aiming to drive a red LED with a constant current IC (NCR401U) when nFAULT is asserted. The final answer confirms the nFAULT pin can sink 500uA, which is insufficient for the desired 5-10 mA LED current. An accompanying answer suggests that sinking a few milliamps is generally safe, but the specific 500uA limit should be adhered to.
AI Generated Content
Category: Datasheet/Specs
Product Number: LTC4365

The LTC4365 looks like a great part for my application where I just want a little extra protection against UV/OV/Reverse Polarity blowing up some of our expensive dev boards. Nominal input voltage range is 7.. 9 VDC so I plan to set the windows from 6.75.. 9.25 VDC.

I'd like to have a red LED light up when FAULT (I'll refer to as nFAULT from now on) is asserted, and was going to use a little external constant current IC to drive the LED, maybe the NCR401U. Rather than add a separate switch / part, I'd like to connect its GND right to the nFAULT pin so it lights up when nFAULT is asserted.

I scanned the datasheet, and I see a spec for leakage current, but not a sink current spec. I see a -1 mA sink spec for UV/OV/nSHDN, but not for nFAULT.

Could someone confirm what sink current is allowed on nFAULT? I would likely do something between 5 and 10 mA.

Edit Notes

added part number to subject
[edited by: movax at 8:38 PM (GMT -5) on 10 Dec 2025]
Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.