Category: Hardware
Product Number: LTC3779
Hello,
I am developing and using an LED strobe driver for vision inspection using LTC3779.
The specifications previously developed using LTC3779 were capable of outputting approximately 50A at 60V output when pulse controlled.
In the newly developed product, we aim to double the existing output current specifications.
I tested two previously developed LED strobe drivers connected in parallel, but I couldn't achieve the desired output.
It seems the output current isn't evenly distributed between the two drivers.
Is there any way to solve this or any booster devices that can be connected in parallel?
Best Regards
Cho