Post Go back to editing

Duty-cycle up to 100%

Thread Summary

The user inquired about using the LT3845A at 100% duty cycle for 300ms to maintain an output voltage equal to the input (24V-32V) before dropping to 15V. The final answer indicated that the LT3845A cannot operate at 100% duty cycle, but suggested the LTC3824 and LTC3864 as alternatives that can. For space applications, the LT8650S can operate up to 99% duty cycle in burst mode, or a prioritizer can manage two voltage sources.
AI Generated Content
Category: Hardware
Product Number: LT3845A

Dear All,

I've a question about maximum duty-cycle of LT3845A.

In our application, starting from a 28V bus (range 24V - 32V), we need an output voltage which is equal to input bus for a definite time (< 300ms) and than goes down to 15V.

Is it possible to use this PWM controller, running it at 100% duty cycle for the first 300ms?

Thanks in advance for your reply.

Kind Regards

Stefano

Parents
  • Hi,

    We are actually studying a solution with two sources and a mosfet system that directs the two voltages, but since this system would have to be applied on 9 distinct lines, the number of mosfets needed is becoming considerable.

    Thank you very much for your support.

    Regards

Reply
  • Hi,

    We are actually studying a solution with two sources and a mosfet system that directs the two voltages, but since this system would have to be applied on 9 distinct lines, the number of mosfets needed is becoming considerable.

    Thank you very much for your support.

    Regards

Children
No Data