Post Go back to editing

Duty-cycle up to 100%

Thread Summary

The user inquired about using the LT3845A at 100% duty cycle for 300ms to maintain an output voltage equal to the input (24V-32V) before dropping to 15V. The final answer indicated that the LT3845A cannot operate at 100% duty cycle, but suggested the LTC3824 and LTC3864 as alternatives that can. For space applications, the LT8650S can operate up to 99% duty cycle in burst mode, or a prioritizer can manage two voltage sources.
AI Generated Content
Category: Hardware
Product Number: LT3845A

Dear All,

I've a question about maximum duty-cycle of LT3845A.

In our application, starting from a 28V bus (range 24V - 32V), we need an output voltage which is equal to input bus for a definite time (< 300ms) and than goes down to 15V.

Is it possible to use this PWM controller, running it at 100% duty cycle for the first 300ms?

Thanks in advance for your reply.

Kind Regards

Stefano

  • Hi,

     

    Unfortunately, the LT3845A does not operate at 100% duty cycle. We do make a couple of similar buck converters that can operate at 100% duty cycle. A couple of examples would be the LTC3824 and the LTC3864. Alternatively, you could look at using a buck-boost converter instead.

     

    Thanks!

  • Hi,

    thank you very much for your gently reply.

    We're looking for a solution that could perhaps also be used in space applications in the future.

    Do you have any PWM controllers you'd recommend?

    Thanks in advance

    Stefano

  • Hi,

     

    For space applications, we currently do not have any converters other than buck converters. That being said, the LT8650S will work in burst mode up to 99% duty cycle. 

     

    If that is still not good enough, you may need to have two voltage sources (the input and the converter output) both connected to your load through some sort of prioritizer, that way you can apply the two separate voltages at different times.

     

    Thanks!

  • Hi,

    We are actually studying a solution with two sources and a mosfet system that directs the two voltages, but since this system would have to be applied on 9 distinct lines, the number of mosfets needed is becoming considerable.

    Thank you very much for your support.

    Regards

  • Hi,

    Regarding the LT3845A, would it be possible to replace the bottom N-channel MOSFET with a freewheeling diode and leave the BG pin "unconnected"?

    Thanks in advance for your reply

    Stefano

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.