KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
LT8650S
Recommended for New Designs
The LT8650S is a dual step-down regulator that delivers up to 4A of continuous current from both channels and supports loads up to 6A from each channel...
Datasheet
LT8650S on Analog.com
Hello,
In order to reduce conducted emission is it recommended to place a 68µH inductor (SRN4018BTA-680M) before EMI filter mentioned in (DC2407A) at the input voltage?
the switching frequency of LT8650S is 2Mhz and by which a CAN interface will be powered.
Thank you!
Hi,
after some experiments I've found that adding a big inductor at the input of LT8650S make it unstable and also has not effect on EMC improvement.
Using LTpowercAD for analysing the power supplie regarding the EMC was a very good suggestion,
thank you so much for your answer.!
Hi,
after some experiments I've found that adding a big inductor at the input of LT8650S make it unstable and also has not effect on EMC improvement.
Using LTpowercAD for analysing the power supplie regarding the EMC was a very good suggestion,
thank you so much for your answer.!