KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
LT8650S
Recommended for New Designs
The LT8650S is a dual step-down regulator that delivers up to 4A of continuous current from both channels and supports loads up to 6A from each channel...
Datasheet
LT8650S on Analog.com
Hello,
In order to reduce conducted emission is it recommended to place a 68µH inductor (SRN4018BTA-680M) before EMI filter mentioned in (DC2407A) at the input voltage?
the switching frequency of LT8650S is 2Mhz and by which a CAN interface will be powered.
Thank you!
Hi,
We recommend a CLC pi filter on the input for EMI suppression, like that shown in the demo board. You do not necessarily need to add another inductor before the pi filter.
Additionally, if you design your converter using LTPowerCAD, there is a tool in the tool bar on the first page that allows you to design your input pi filter and visualize the conducted EMI for different standards. It looks like this when you load the design tool for the LT8650S:
Thanks!
Hi,
after some experiments I've found that adding a big inductor at the input of LT8650S make it unstable and also has not effect on EMC improvement.
Using LTpowercAD for analysing the power supplie regarding the EMC was a very good suggestion,
thank you so much for your answer.!