Post Go back to editing

Evaluation board - difference between DC2665A-B and DC2665B-B

Thread Summary

The user inquired about the redesign of the DC2665A to DC2665B evaluation board, focusing on the addition of input-side capacitance (C29) and layout changes. The final answer explained that the redesign aimed to reduce noise coupling from Vin to Vout by decreasing board dimensions, optimizing capacitor placement, and separating Vin and Vout copper areas. The changes also reduced output voltage ripple, particularly at the board's edge, and supported the LTM4657 (-C variant) buck converter.
AI Generated Content
Category: Hardware
Product Number: LTM4638

The DC2665A (circa 2018) was replaced by the DC2665B (circa 2022) as the reference design/eval board for the LTM4626, LTM4638, and LTM4657 buck converters.

These two designs (DC2665A, DC2665B) are largely identical, except:

  1. The DC2665B also supports the LTM4657 (-C variant),
  2. There is additional output-side capacitance,
  3. There is additional input-side capacitance (particularly C29, the "fast" .022uF 0603), and
  4. The layout has changed significantly.

Item (1) is sensible and item (2) is explained by the revision history section in the DC2665B manual ("DC2665B-B replaces DC2665A-B for low HF VOUT ripple.")

I'm curious specifically about the input-side capacitance (3) and associated layout changes (4). Why was the EVB redesigned, and why was C29 added? I understand why fast capacitance is necessary at the input side and should have been present on the DC2665A, but I'm wondering if you can describe the actual impact its absence had on the DC2665A and whether this is the reason for the re-design.

  • The evaluation board was mainly revised to address noise coupling from Vin to Vout. The board dimensions were decreased, the Vin and Vout copper areas were reduced and these areas are separated from being side by side.  Additionally, the input capacitor placement and vias were optimized to reduce the hot-loop and output capacitor placement was optimized to reduce output voltage ripple especially at the edge of the board.