Post Go back to editing

Simulation

Category: Hardware
Product Number: LT1129IS8TRPBF, LT1129

Hi Team,
I simulated my circuit with Vin = 28 V and I need Vout = 15 V.
I used R1 = 5 kΩ and R2 = 15 kΩ, but the output voltage is only 7 V.


I downloaded the two models from the link and built the circuit accordingly.

Regards,
Rami Reddy.

  • Hi Rami,

    Thank you for reaching out to Analog Devices!

    For your application, please use the LT1129 rather than the LT1129-5. The LT1129 is the adjustable version, which allows you to set different output voltage levels as required. In contrast, the LT1129-5 is the fixed 5V output version.

    • LT1129 → Adjustable output
    • LT1129-5 → Fixed 5V output

    For your convenience, I’ve included the LTspice schematic and reference image in the link below:

    Please let me know if you have any further questions or need additional support.

    Thanks and Regards,
    Tech Support