Hi,
I am planning to use MAX17651 LDO for my project where I need precise (+/- 0.01V) output voltages. The datasheet gives a formula to calculate the top resistor located on the resistor divider. But this formula assumes you are using a 59 kOhms resistor on the bottom side of the resistor divider. The datasheet also does not mention the Feedback input leakage current effect on the output resulted with the following formula:
My question is, can I use the below formula which is typically mentioned on every other ADI LDO's to calculate the output voltage and is it OK to use this LDO for such precise output voltage requirement?
Edit Notes
Added more tags to the post.[edited by: ehali at 12:03 PM (GMT -5) on 25 Nov 2025]