Post Go back to editing

Negative Output Considerations

Category: Datasheet/Specs
Product Number: LTM8050
Software Version: -

I designed a circuit using the LTM8050 with a +28 V input and a -15 V output. I directly connected the AUX and BIAS pins. However, I heard that when generating a -15 V output, the datasheet requires an additional configuration using a resistor and a Schottky diode.

What happens if this is not implemented?

Also, if a problem occurs, could the 4.7 µF / 100 V capacitor on the 28 V input side be damaged?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.