I want to use the ADP163 LDO for output voltages greater than 4.2V.
The input voltage range is 2.2V to 5.5V. The maximum drop-out voltage is 225mV (TSOT-package) @ 150mA and full temperature range (= worst case scenario).
If the input voltage is e.g. 5.2V and the desired output voltage is e.g. 4.8V why shouldn't this be possible?
What does cause the limitation to 4.2V for the allowed output voltage?
Is this information in the datasheet correct (ADP160-163 datasheet Rev. H, page 12) ?
Your comment is highly appreciated. Thanks in advance !
Regards,
Ferdinand.