Hello Guys,
The LTC4370 does the job for what i require but it has some restrictions for my application which are:
- It is not AEC-Q100 Qualified
- It does not support operating temperature range of -40C TO +125C
In total I need an load sharing controller which supports
- Voltage difference from two power supply inputs
- AEC-Q100 Qualified
- Operating temperature range of -40C TO +125C
- Vin min - 3.2volts or less
- Vin max - 13volts or more
- It should be SMD type not through hole type
- Internal or external MOSFET does not matter
- Dual channel or Single channel does not matter (I will use two if it is single channel)
So, I'am not able to find one controller with this features added
It would be good if you guys recommended me one with all the above features
Thank you,