Post Go back to editing

LT8705 inverting buck-boost

Category: Hardware
Product Number: LT8705HFE, LT8705
I am designing a DCDC buck-boost converter using LT8705H.

The circuit configuration is as follows.

I'm designing a 28V input with two channels of +15VDC and one channel of -15VDC output.
There are no issues with the outputs, but when connected as shown below, the -15VDC output does not occur.


However, when the input voltage is varied by 2-3V while ON, or when the input is turned OFF and then immediately turned ON, the output is -15VDC.
I'm using the LT8705.

I've read the datasheet, but I can't find the cause of the problem. I'd appreciate your feedback and suggestions for a solution.

Current testing is being done under no-load conditions.



Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.