Post Go back to editing

How to connect two LT3935 in parallel to supply about 5A to LED strip?

Category: Hardware
Product Number: LT3935

Dear Sir,

We are going to design some led driver board with LT3935.

==================================================================

Design conditions as the below:

1. Input voltage: 36V

2. LED strip current: 5A / 33V

==================================================================

Here's our question

==================================================================

1. How to connect two LT3935 in parallel to supply about 5A to LED strip?

    Is it possible? Or, do we need additional component?

    please, let me provide the sample schematic.

2. In the datasheet, input voltage is Max. 36V 

   Our supply voltage is about 36.36V

   is it too high? 

   If we supply voltage 36.36V to LT3935, it may be damaged?

==================================================================

Please let me guide.

Thanks and best regards,

Kwangbog Ham

Parents Reply Children
No Data