Dear Sir,
We are going to design some led driver board with LT3935.
==================================================================
Design conditions as the below:
1. Input voltage: 36V
2. LED strip current: 5A / 33V
==================================================================
Here's our question
==================================================================
1. How to connect two LT3935 in parallel to supply about 5A to LED strip?
Is it possible? Or, do we need additional component?
please, let me provide the sample schematic.
2. In the datasheet, input voltage is Max. 36V
Our supply voltage is about 36.36V
is it too high?
If we supply voltage 36.36V to LT3935, it may be damaged?
==================================================================
Please let me guide.
Thanks and best regards,
Kwangbog Ham