Post Go back to editing

LT8610AB - vout less than 3.3V

Thread Summary

The user asked about connecting the BIAS pin when Vout is less than 3.3V, such as 1.8V. The final answer confirms that an alternate supply can be connected to the BIAS pin, and suggests referring to page 10 of the datasheet for more details. The accompanying answers clarify that the LTPower simulation requires Vout to be above 3.1V, and ask if 3.3V from another supply can be used for the BIAS pin when Vout is below 3.1V.
AI Generated Content
Category: Hardware
Product Number: POWER

Hello

 

If the Vout is less than 3.3V, for example 1.8V, How I need to connect the Bias pin?

 

Roi

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.